Avnet Technology Solutions


Home

Sales

Software Downloads

On-Line Documentation

         
 

SavWareHA Administration Menu

The SavWareHA administration menu can be started by logging on to the ‘root’ account and entering the command ‘sentinel’. If no mirrors are configured, only the ‘Utilities’ option will be displayed. Sub-menus can be selected for each mirror and for ‘Utilities’ by using either the arrow keys or [SPACE] (space bar) to move the ">" pointer to the desired selection and pressing [RETURN].

SavWareHA Menu Keystrokes

The following keystrokes can be used while in the SavWareHA administration menu:

 

Ý, ß (Up/Down Arrow)

Move Selection Pointer to Next/Previous Option

[SPACE] (spacebar)

Move Pointer to Next Option

[RETURN]

Execute Option at Pointer

[END], [ESC], [CONTROL-E]

Exit Current Menu, Abort Current Entry

[CONTROL-R]

Repaint Current Screen

Ü “, “Þ (Left/Right Arrow)

Move current sub-window left/right

“U”, “u”, “D”, “d” keys

Move current sub-window up/down

[BACK-TAB]

Move to previous input

[F3 ]

Generate and choose a response from a list of options


SavWareHA Administration Screen

Each mirror will consist of a pair of mirror element boxes, the Primary System shown on the left, and the Standby System shown on the right. Underneath the mirror description (‘Mirror 0’ above) is shown the device name (‘/dev/mirror00’ ), and its size (1461Mb). The system status (‘Normal Operation’, ‘On stmain ’) is shown in the upper right hand corner of the screen.


SavWareHA Screen Definitions


Mirror Status Codes

The mirror status codes are located in the upper right hand corner of each mirror side’s display box. See the ‘Specific Error Recovery Procedures’ section in this manual for more information.

ACTIVE Mirror is GOOD and in use. The mirror is currently mounted.
 
CHECK An unknown error was encountered while getting the status of the mirror . Usual indications are network or device errors or misconfiguration of mirror devices. Removal and rebuilding of the mirror (not SavWareHA itself), or testing of the network connection is the suggested remedy.
COLD The element data is valid as of the date displayed. The element can be updated manually via the Regenerate Mirror option. Usually reserved for either root mirrors or for inactive (archival) data mirroring.
 
DISK ERROR A disk error has been reported on the mirror device. The mirror has been broken. Correct the hardware problem and regenerate the mirror with the ‘Fix Broken Mirror: Regenerate Mirror’ selection.
 
ERROR An error was encountered while trying to access the mirror device. Correct the network communication error(s) and regenerate the mirror with the ‘Fix Broken Mirror: Regenerate Mirror’ selection.
 
GOOD Mirror is GOOD but is not in use. The mirror is not currently mounted.
 
MISMATCH The date & time codes are different on the mirror elements. This usually occurs when some of the controlling files in either ‘/etc/default’ or ‘/etc/sentinel.d’ have become corrupted; or may reflect misconfiguration of mirror devices. Removal and rebuilding of the mirror (not SavWareHA itself) is the suggested remedy.
 
NEED REGEN Mirror side requires regeneration . No reads are enabled on the destination mirror element.
 
NOT CLOSED The system was not shutdown properly. The mirror must have ‘fsck ’ run on the mirror device after regeneration has started. Until both regeneration and a successful ‘fsck’ has occurred, the mirror will not be accessible.
 
NOT SETUP The drive has not been setup for a mirror . This usually means that the SavWareHA configuration files expected to find a mirror stamp on the device, but did not.

 

 
         
         
 

This site is governed by Avnet, Inc.Terms and Conditions, Legal Notices & Privacy Statements.
Copyright © 1996-2005 Avnet, Inc. All rights reserved.