|
Registration - reggie
The
SavWareHA Software must be registered within 30 days of installation.
The serialized SavWareHA product will be fully functional for this
grace period. Use the SavWareHA Registration option from the Utilities
menu to display the Registration Request string and to perform the
product registration . The Registration Request string must be transmitted
to the central registration system and a Registration Code will
be returned. The Registration Code must be entered into the system
to allow the SavWareHA software to continue to operate.
Registration
Procedure
The registration
procedure is designed to be as easy as possible. Use any of the
following ways to register:
- FAX:
The program will generate the Registration Request and send it
to the customer support fax number via a Unix fax system. A fax
system such as VSI*FAX or True Fax must have been previously installed
and configured on the system. When the fax is received by the
central registration system, it will generate the Registration
Code and return it via fax, e-mail, or voice as appropriate.
- E-Mail:
The program will generate the Registration Request and send it
via electronic mail to the central registration system at reggie@avnet.com.
An e-mail package must have been previously installed and configured
with a connection to the Internet. The Registration Code will
be returned via e-mail to the originating system.
- Print:
The program will print the Registration Request to a printer.
The request may be faxed or mailed to the central registration
system. The registration code will be faxed back to the fax number
as displayed on the fax request. Make sure that the return fax
number is correctly and clearly indicated on the initial fax or
letter.
- File
: The Registration Request can be written to a file and then transmitted
to the central registration system via any means possible. The
return contact information must be supplied for the Registration
Code.
When the Registration
Code is returned from the central registration system, it can be
entered electronically (Direct Modem), entered manually through
the keyboard or read in from a file.
Central
Registration System Information
Avnet
Technology Solutions
Voice
(480) 794-2700 Option 2 then 5; FAX (949) 789-4365
E-mail
: reggie @avnet.com
WWW:
http://www.savwareha.com/downloads/registration.asp
|