|
SavWareHA
Sub-Menus
Mirror
Sub-Menu
This menu will be enabled when the selector is moved by pressing
either Ý , ß , or [SPACE] keys
to position the highlight pointer at a mirror and [RETURN] is pressed.
The options executed from this menu only affect the mirror selected
(except for display mirror log which shows entries for all mirrors
on the system).

Each of these
selections are described in detail on the following pages. Please
note that only the system administrator should access these selections.
Display Mirror Status
This selection
allows the user to examine the status flags for each side of the
mirror. Also, information as to the creation and last access dates
and times are shown, and the size of each mirror side.
This screen
will show the protocol for the data link (TCP/IP or LLI) when both
sides of the mirror are active.
Fix Broken Mirror
This
selection displays another menu whose three selections are shown
below:

This menu controls
the fixing, or regeneration, of a broken mirror; allows
the user to turn off the Standby System element or the mirror selected.
By pressing [END], [ESCAPE], or q, the user may exit
this menu without making a selection.
Each of these
options is explained below, with representative screen displays.
Regenerate Mirror
[Use With
Caution!]
Use this option
to bring the mirror back into compliance after some error has either
broken the mirror completely (either the master or slave side of
the mirror has been turned OFF intentionally or by the
action of the mirror driver), or one side of the mirror reported
a read or write error (usually resulting in the offending sides
read/write flag being set to W rite only), or when the
Primary System is unable to reach the Standby System (the slave
side of the mirror will then display ERROR).
The program
will display the mirror elements again, and will prompt the user
for authority to begin a regeneration from the GOOD
or ACTIVE side of the mirror to the inactive side of
the mirror. An affirmative (y) response will immediately
begin the regeneration; any other response will abort the regeneration.

Always check
the direction of the copy to insure that valid data will not be
inadvertently overwritten.
Turn Off Standby Element
[Use with
Caution]
This options
effect is to turn off all reads and writes to the slave (Standby
System) side of the mirror. No system interruption will be noticed
by the users on the Primary System. All pending disk writes will
be flushed, no more writes (or reads) will be accepted. The slave
sides status will be set to OFF.
Some circumstances
where the user may wish to use this option: The Standby System must
be taken completely away; a verified backup of the mirrored unit
in a quiescent state is desired without interrupting the Primary
Systems users; some impending Standby System, network error
or major reconfiguration is anticipated in the near future.
Note that this
will pause the SavWareHA monitor program on the Standby system.
No further mirroring will be done, and no automatic fallback process
will be initiated. Use the Fix Broken Mirror: Regenerate Mirror
option to bring the mirror back into compliance.

Turn Off Primary Element
This
options effect is to turn off all reads and writes to the
Primary Systems side of the mirror. No system interruption
will be noticed by the users on the Primary System. All pending
disk writes will be flushed, no more writes (or reads) will be accepted.
The Primary Systems status will be set to OFF.
Some circumstances
where the user may wish to use this option: The Primary Systems
disk array must be taken completely away (assuming there are hot
swap drive carriers in use); some impending system threatening
error is about to occur if the Primary Systems side of the
mirror is left active for either reading or writing.
Note that this
will NOT pause the SavWareHA monitor program on the Standby system.
No further mirroring will be done on the Primary System - all reads
and writes will be performed on the Standby System over the data
link connection. Use the Fix Broken Mirror: Regenerate Mirror
option to bring the mirror back into compliance.

Check Mirror Integrity
[USE CAUTION!]
NOTE: This option
was removed in Revision 2.01a of SavWareHA, and is included here
for those installations prior to Revision 2.01a.
This option
will allow dynamic block by block comparison of the mirrored units.
Please note that on an active filesystem there may be some errors
reported by this option. This is due to the fact that the mirror
reads on either side may be dynamically interrupted by a write buffer
flush before both sides blocks have been read, thereby reporting
an error that does not really exist. For this reason, only use this
option when the mirror is quiescent (unmounted).
Change Read Flags
[USE CAUTION!]
This option
will allow the user to toggle on or off the read enabling flags
for either side of the mirror. Care should be taken when using this
option, as system performance may be impacted (in the case of turning
on reads to both sides of the mirror)..

|