|
System Requirements
Operating Systems
- SCO Unix
3.2v4.0 (or later) with TCP/IP 1.2
- SCO Open
Desktop Version 2.0 (or later)
- SCO Enterprise
Server
- SCO OpenServer
5
- SCO UnixWare
7
The general
requirement is that each machine have SCO Unix 3.2v4.0 (or later),
and TCP/IP version 1.2 (or later) installed.
Disk Space
SavWareHA will
take approximately 1 megabyte of disk space on the root filesystem
of each system for the programs and configuration files. Also, disk
partitions of equal block size must be defined on each machine to
provide a mirror of the user data.
Note: Because
SavWareHA requires two fully functional SCO Unix operating systems
(one on the Primary and one on the Standby), the root filesystem
cannot be mirrored between the two systems. User accounts, printer
setup and other configuration information can be automatically duplicated
on each system using the /etc/mracdb functionality. Refer to the
appendix for detailed instructions.
Memory
SavWareHA will
use approximately 60Kb of memory during normal operation. An additional
16Kb will be used during a regeneration.
Network Cards
In addition
to requiring SCO TCP/IP, any network card supported by the SCO LLI
(Link Level Interface) Drivers or SCO TCP/IP can be used by SavWareHA.
Refer to the SCO Hardware Compatibility Guide for a
detailed list of supported network cards. One network card is required
in each system for the data mirroring. Additional network card(s)
connecting to separate networks are recommended if users on the
system will be using networking devices and software.
Serial Device Connection
A terminal server
(either Ethernet based, or using a proprietary connectivity scheme)
is required if serial devices (printers, terminals, modems, and
the like) are going to be connected to the SavWareHA systems
IO Link and are to be switched automatically to the Standby System
if a failure occurs. Any multi-host capable serial connectivity
scheme, such as the Equinox SST, that is supported under SCO Unix
may be used.
|